Output Amplitude
Set the output amplitude in Vpp.
Parameter choices vary by instrument. Some of the parameters listed below might not be available on your particular instrument. The application will list only those parameters, and parameter ranges, available for your particular instrument.
You can also set the amplitude (with an associated offset voltage) by specifying a High Level and Low Level. For example, if you set the high level to +2 volts and the low level to -3 volts, the resulting amplitude is 5 Vpp (with an offset voltage of -500 mV).
To set the High Level, click the "Amplitude" drop-down and select "High Level".
To set the Low Level, click the "Offset" drop-down and select "Low Level".